Choosing the best Xsens mocap setup is not always as straightforward as we like it to be. Different options, requirements, and challenges will be based on each individual's situation.
This is why we've put together this guideline: to help you make the best decision for your situation.
Did you already make your choice on going forward with Xsens? If not, we have resources available for you to look at, like an overview of comparisons and reviews of motion capture providers by the community and an overview of productions powered by Xsens.
Now that you are convinced Xsens is the best solution, we can help you select the best setup for your specific situation.
In general, you have to make four choices:
Let's dive into these three questions one by one.
Inertial motion capture requires sensors that are attached to the body in order to capture your movements. Xsens has developed a wireless sensors setup (Xsens Awinda) and a tethered sensors setup (Xsens Link). Both setups use 17 sensors, while Xsens Awinda has wireless sensors fitted on the body with adjustable straps that allow for fast, easy, and reliable motion capture. Xsens Link's sensors are fitted on the body through a Lycra suit ensuring even more accurate data recording.
Note: The connection from the body to the computer is always wireless.
What is the best choice for me, Xsens Link or Xsens Awinda (Starter)?
Choosing between Xsens Link and Xsens Awinda (Starter) depends on your goal with motion capture. For further inspiration, here is an overview you can use to pick the best hardware for your situation:
MVN Link | MVN Awinda (Starter) |
For high-impact mocap shoots, like rough fights | When you have several actors using the same setup |
Large groups of motion capture (with OBR) | Ideal for regular motions, nothing too rough |
When using positional aiding (GPS/HTV Vive) | Can be worn over your regular clothing |
When you need a large range (up to 150 m) | The range is 20 to 50 m |
When you need high framerates (240 Hz) | Maximum of 60 Hz framerate |
Go to Xsens Link product page | Go to Xsens Awinda product page |
In addition to the Link and Awinda, we have the Awinda Starter. So, in total, we have three different hardware options:
Once you have chosen your hardware, the next step is to determine the software subscription that best suits your goals. Xsens offers three subscription types, each supporting a different use of our motion capture systems. The two versions are Xsens Animate Live and Xsens Animate Pro.
HD Reprocessing gives you the best quality motion capture data available in the market. The data is processed using our proprietary HD Reprocessing Engine and takes the motion capture data to a whole new level of accuracy and smoothness.
Do I choose Xsens Animate Live or Pro?
The main differences between the Animate Live and Pro subscriptions are based on your intention with motion capture. Consider these questions when making the best choice for the subscription:
Not everyone uses motion capture throughout the year. There are many studios that only use mocap during specific projects. For this, we offer limited-time subscriptions and other options to fit your approach.
Animate Live | Animate Pro | |
3-months | X | |
6-months | X | |
1 year | X | X |
3 year | X | X |
Your Xsens motion capture setup is now complete for use. However, there are additional services and hardware you might need to optimize your pipeline or add additional data.
Think about these options:
For Indie studios we have the Xsens Indie Program, a program to support up-and-coming talent, making it easier to access Hollywood-grade motion capture on a budget. the program is designed to support a more affordable way to bring projects to life, without having to compromise on quality.
The Xsens Indie program is available to you if you meet the following criteria:
Reach out to us for further information.
Now that you have been informed about all the different options and features Xsens offers, you are ready to order.
To get this started, click on the button below and fill out your order details. We will provide you with an overview and quote as soon as possible.