Choosing your mocap setup
Choosing the best Xsens mocap setup is not always as straightforward as we like it to be. Different options, requirements, and challenges will be based on each individual's situation.
This is why we've put together this guideline: to help you make the best decision for your situation.
Did you already make your choice on going forward with Xsens? If not, we have resources available for you to look at, like an overview of comparisons and reviews of motion capture providers by the community and an overview of productions powered by Xsens.
Now that you are convinced Xsens is the best solution, we can help you select the best setup for your specific situation.
In general, you have to make four choices:
- What hardware do I need?
- What software do I need?
- Do I need additional services or hardware?
- Do I use mocap all year long, or project-based?
- Are you an Indie?
- How do I order?
Let's dive into these three questions one by one.
What Xsens hardware do I need?
Inertial motion capture requires sensors that are attached to the body in order to capture your movements. Xsens has developed a wireless sensors setup (Xsens Awinda) and a tethered sensors setup (Xsens Link). Both setups use 17 sensors, while Xsens Awinda has wireless sensors fitted on the body with adjustable straps that allow for fast, easy, and reliable motion capture. Xsens Link's sensors are fitted on the body through a Lycra suit ensuring even more accurate data recording.
Note: The connection from the body to the computer is always wireless.
What is the best choice for me, Xsens Link or Xsens Awinda (Starter)?
Choosing between Xsens Link and Xsens Awinda (Starter) depends on your goal with motion capture. For further inspiration, here is an overview you can use to pick the best hardware for your situation:
MVN Link |
MVN Awinda (Starter) |
For high-impact mocap shoots, like rough fights |
When you have several actors using the same setup |
Large groups of motion capture (with OBR) |
Ideal for regular motions, nothing too rough |
When using positional aiding (GPS/HTV Vive) |
Can be worn over your regular clothing |
When you need a large range (up to 150 m) |
The range is 20 to 50 m |
When you need high framerates (240 Hz) |
Maximum of 60 Hz framerate |
Go to Xsens Link product page |
Go to Xsens Awinda product page |

In addition to the Link and Awinda, we have the Awinda Starter. So, in total, we have three different hardware options:
- Xsens Awinda Starter
Straps - Wireless Sensors - Short range
This is the best entry-level hardware option. You get a full-body Awinda set with USB dongle receiver.
- Xsens Awinda
Straps - Wireless Sensors - Longer range
If you need more range, this hardware option is the best fit. You get a full-body Awinda set with a professional Awinda station and charging station.
- Xsens Link
Lycra suit - Embedded Sensors - Full options
Our flagship MVN Link suit gives you an even bigger range, higher update rate and lower latency. It also comes with many extra features such as On-Body Recording and HTC Vive integration.
What Xsens software do I need?
-1-1.png)
Once you have chosen your hardware, the next step is to determine the software subscription that best suits your goals. Xsens offers three subscription types, each supporting a different use of our motion capture systems. The two versions are Xsens Animate Live and Xsens Animate Pro.
HD Reprocessing gives you the best quality motion capture data available in the market. The data is processed using our proprietary HD Reprocessing Engine and takes the motion capture data to a whole new level of accuracy and smoothness.
Do I choose Xsens Animate Live or Pro?
The main differences between the Animate Live and Pro subscriptions are based on your intention with motion capture. Consider these questions when making the best choice for the subscription:
- Are you streaming live?
Live streaming is only possible with Xsens Animate Live and Pro. Live streaming or Vtubing is possible with Animate Live, and streaming a virtual optical marker set is only available in Animate Pro.
- Do I need HD Reprocessed data?
The best quality motion capture data using the HD Reprocessor is only available in Xsens Animate Pro.
- How many actors will you be capturing?
You can Animate Live to supports two actors and Animate Pro supports multiple or even unlimited actors if you use On-Body Recording.
- In what formats do you want to export your files?
You cannot export files in Xsens Animate Live. In Animate Pro you can export locally to MVNX, FBX, BVH and C3D.
- Are you using third-party plug-ins?
Third-party plug-ins from Unreal Engine, Unity and Autodesk are only available for Animate Pro.
- Are you using additional positional aiding?
Integration with positional aiding hardware such as HTC Vive and GPS is only available in Animate Pro.
- Are you using the extra features of the MVN Link suit?
If you will be using the (Remote) On-Body Recording feature, you need the Xsens Animate Pro.
Do I use mocap all year long, or project-based?
Not everyone uses motion capture throughout the year. There are many studios that only use mocap during specific projects. For this, we offer limited-time subscriptions and other options to fit your approach.
|
Animate Live |
Animate Pro |
3-months |
|
X |
6-months |
|
X |
1 year |
X |
X |
3 year |
X |
X |
Do I need additional services or hardware?

Your Xsens motion capture setup is now complete for use. However, there are additional services and hardware you might need to optimize your pipeline or add additional data.
Think about these options:
- Finger Tracking
Xsens Metagloves by MANUS
Adding finger tracking is possible with the MVN Gloves by MANUS which have a native integration in all subscriptions. More about the Xsens Metagolves gloves here.
Xsens Prime 3 by Manus
Convey every single emotion through precise finger movement tracking, fully and natively integrated with Xsens mocap. More about the Prime 3 here.
StretchSense
You can integrate finger tracking with StretchSense in MVN Animate Plus and Pro.
- Facial Capture
There are several resources online on how to get facial data into Unreal, Unity, iClone or Maya:
Via an iPhone using the Live Link Face app
Via a professional system such as Faceware
- Additional or replacement mocap accessories
You can order additional prop sensors, straps, suits, backup sets, and more in our online shop. Visit our online shop here.
- HTC Vive base station and trackers
To use additional positional tracking of actors or objects, you can use HTC Vive. We have an integration available in the MVN Animate Pro subscription. Find out more about how to do the integration here.
Are you an Indie?
For Indie studios we have the Xsens Indie Program, a program to support up-and-coming talent, making it easier to access Hollywood-grade motion capture on a budget. the program is designed to support a more affordable way to bring projects to life, without having to compromise on quality.
The Xsens Indie program is available to you if you meet the following criteria:
- You are a new Xsens customer
- You have a registered company (CoC, VATno)
- Your revenue over the last fiscal year is no more than $550,000 (€500.000)
Reach out to us for further information.

How do I order?
Now that you have been informed about all the different options and features Xsens offers, you are ready to order.
To get this started, click on the button below and fill out your order details. We will provide you with an overview and quote as soon as possible.