Authors: Faber GS1,2, Chang CC2, Kingma I3, Dennerlein JT1
1 Department of Environmental Health, Harvard School of Public Health, Boston, MA, USA
2 Liberty Mutual Research Institute for Safety, Hopkinton, MA, USA
3 Research Institute MOVE, Faculty of Human Movement Sciences, VU University Amsterdam, The Netherlands
Biomechanical overexposure is a risk factor for occupational injuries. Therefore, it is important to evaluate the biomechanical exposure in the workplace. Methods currently used, such as video analysis, are time-consuming and therefore not frequently used.
This poster presents a less laborious wearable measurement system for automatic and continuous ambulatory assessment of joint loading in the occupational setting.
The wearable measurement system (Xsens Technologies, Netherlands) consists of: 1) a full body inertial sensor motion capture system (measuring segment orientation) which can be worn under the clothes and 2) shoes instrumented with 3D force sensors. Using this system you are able to assess not only joint loading due to body postures, but also joint loading due to external loads (using the forces measured by the shoes), occurring during manual materials handling, for example.
In recent studies we have successfully validated separate components of the proposed measurement system:
Currently we are validating the combined measurement system in the laboratory by comparing the assessed joint loading to that of a conventional state-of-the-art lab-based method. If the proposed system proves to be a valid measurement system, we will use it in future field studies.
Are you interested our solutions? Please click on the button below to contact us.