Autonomous vehicles
Movella motion tracking solutions are being used in an ever-growing range of non-consumer, land-based autonomous vehicles.

Driving new autonomous vehicles and motion tracking applications
Movella motion tracking solutions are being used in an ever-growing range of non-consumer, land-based autonomous vehicles. Think, for example, of off-road vehicles, robots, or goods and people transporters in closed areas such as airports, marine ports, large industrial sites, or campuses. Unlike consumers in the automotive market, our customers in these application areas are driven less by regulatory considerations, and more by specific performance needs.

The road to safety, efficiency, and reliability
A vehicle can only operate autonomously if it knows where it is, where it’s going, and how to get there. That’s why autonomous vehicles are often equipped with a large variety of sensors, including cameras, lidar, GNSS, and wheel odometry.
However, each of these sensor solutions has its downsides:
- Cameras and lidar are expensive, power-consuming and affected by weather, sight limitations and vibrations
- GNSS has a low update rate and is unreliable in urban canyons and tunnels
- Wheel odometry suffers from wheel slipping and drift.
Fitting a sensor which provides information on the vehicle’s state, irrespective of the environment surrounding it, can help alleviate many of these challenges.
Autonomous vehicle products
Our Motion Tracker Industrial-grade (MTi) product series is based on over 10 years of research & development, hands-on experience, and innovative drive – and comes with global 24/7 tech support. The range of our sensor modules offers exceptional data accuracy and precision, plug and play configurability, and the market’s best performance-to-price ratio.

The MTi-670G combines orientation data with position data supplied by an internal GNSS receiver.
-jpg-2.jpeg)
The MTi-680 represents the highest standard in GNSS/INS when connected to an external Real-Time Kinematic (RTK) GNSS receiver.

With the MTi-680G’s added RTK feature, you can improve your positional data from meter-level to centimeter-level accuracy.
.jpeg)
The MTi-G-710 is an IMU and GNSS/INS with an extra SMA connector, enabling you to connect a GNSS antenna.
Newsletter
Sign up here for the Movella newsletter and stay up to date about everything Movella has to offer.